DCS wiring and programming example

This example complies with ISO 13849-1, Category 4 operation. The standard control portion of the application is not shown.
DCS Wiring Example
This programming diagram shows the Dual Channel Input Stop (DCS) instruction with inputs and test outputs.
DCS Programming exmaple
Ladder Diagram
DCS_Ladder Diagram_wire and program
The programming software is used to configure the input and output parameters of the
Guard I/O
module, as illustrated.
Module Definition
DCST_other_Pg72_v31
Rockwell Automation
suggests selecting
Exact Match
for the
Electronic Keying
as shown. You can also select
Compatible Match
.
Module Input Configuration
DCST_other_Pg73_1_v31
Module Test Output Configuration
DCST_mod test output_v31
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.