SMAT wiring and programming example

The standard control portion of the application is not shown.
Wiring Diagram
SMAT Wiring diagram
Programming Example
The following programming diagram shows the instruction with inputs and outputs.
SMAT Programming example
Ladder Diagram
L5K_SMAT_other LD_v31
The programming software is used to configure the input and output parameters of the
Guard I/O
module, as illustrated.
Module Definition
SMAT_mod_definition_v31
Rockwell Automation
suggests selecting
Exact Match
for the
Electronic Keying
as shown. You can also select
Compatible Match
.
Module Input Configuration
SMAT_mod input cofig_v31
Module Output Configuration
SMAT_module output config_v31
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.