Special Instructions
The special instructions perform application-specific operations.
Available Instructions
If you want to: | Use this instruction: |
---|---|
Compare data against a known, good reference and record any mismatches. | |
Compare data against a known, good reference, record any mismatches, and update the reference to match the source. | |
Pass the source data through a mask and compare the result to reference data. Then write the source into the reference for the next comparison. | |
Control a PID loop. |
Provide Feedback