Remove All Project Documentation overview

Remove All Project Documentation overview

Remove a language localization that is currently in the project. Use the Language to Remove parameter to select the language localization you would like to remove. Only the languages that have content are listed. All the project documentation for the selected language will be removed and the custom languages will be deleted.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal