Founded in 1929 by Swiss immigrants Alfred Nef and Alfred Gozenbach, Valley Queen is a dairy manufacturer in Milbank, South Dakota. Valley Queen can produce 200 million lbs. of cheese from 2 billion lbs. of milk annually into a variety of natural cheeses, dried lactose, WPC80 and anhydrous milk fat, which are marketed and used by private-label and nationally branded food companies.
As one of the largest cheese producers in South Dakota and the largest employer in Milbank, Valley Queen gets milk from roughly 40 area farms, which supports the production of 500,000 lbs. of cheese per day.
In 2018, the company announced a $52-million expansion plan to increase processing capacity by 25% to more than 5 million lbs. of milk per day. The expansion project took place within Valley Queen’s existing footprint at the Milbank facility. By upgrading capital equipment and infrastructure, the company could maximize the existing operating systems and fund new technologies.
As part of this investment, the company hired more than 25 employees to handle the increase in manufacturing capacity, and currently has more than 300 associates.
As Valley Queen invested in its expansion, the need for efficient processes and effective communication became clear.
Before updating the plant-floor communication process, control room operators would view human-machine interface (HMI) screens from Rockwell Automation FactoryTalk® View Site Edition (SE) HMI and manually contact maintenance and operations via PTT on their Motorola analog two-way radios whenever an alarm occurred. Manually processing data was inefficient, and it caused unresolved alarms and unplanned downtime, which negatively affected overall production.
Discovery at the Automation Fair Event
In 2017, several Valley Queen automation and IT staff attended the Automation Fair® event hosted by Rockwell Automation, looking for an innovative communication solution that would maximize their investment in Rockwell Automation hardware and software.
After attending numerous technical sessions, including the joint presentation by Rockwell Automation Encompass™ Product Partners Motorola Solutions and our company SeQent, Valley Queen asked SeQent to update its plant-floor communication process. Valley Queen uses our notification platform to build a software bridge between their Rockwell Automation HMI/SCADA environment and Motorola Solutions MOTOTRBO™ two-way radios.