By Dave Scheuerman, technical training manager, Littelfuse Inc., Industrial Business Unit
When operating in its current-limiting range, a current-limiting fuse is designed to clear a short circuit current in less than one half cycle. Current-limiting fuses operating in their current-limiting range will limit the maximum instantaneous peak (Ipeak) current to a value substantially less than the peak current that could flow if the fuses weren’t in the circuit.
To increase the short-circuit current rating (SCCR) and reliability of industrial control panels (ICPs) while simultaneously increasing the safety of electrical workers, it’s recommended that you do the following:
• Use components or approved combinations with higher SCCRs.
• Use current-limiting fuses or other current-limiting components in the feeder circuit (refer to UL® 508A Supplement SB for more information).
• Use overcurrent protective devices with higher interrupting ratings in branch and control circuits.
• Submit the panel to UL or another nationally recognized testing laboratory (NRTL) for approval testing using the testing method.
Every component within an ICP must be designed to perform in the worst-case scenario, which helps verify people and equipment remain safe should an incident occur.
Currently, UL 508A Supplement SB does not use the apparent root mean square (RMS) let-through voltage of current-limiting overcurrent protective devices to determine the SCCR of industrial control panels. Instead, the supplement compares the UL maximum allowable Ipeak let-through current during the first half cycle of current-limiting fuses with the RMS SCCR of the various components used within the panel.
Current-limiting fuses can optimize a panel as long as the SCCR is considered in its design. Most molded case circuit breakers can’t provide adequate SCCRs. Traditionally, the best way to increase the SCCR of a panel with a low rating has been to switch from a molded case circuit breaker to current-limiting fuses. But after switching to current-limiting fuses, how do you improve the panel’s SCCR even further?
How Does Current Limitation Increase SCCRs?
According to NEC® Article 240.2, a current-limiting overcurrent protective device interrupts currents in its current-limiting range, thus reducing the current flowing in the faulted circuit to a magnitude substantially less than that obtainable in the same circuit if the device were replaced with a solid conductor having comparable impedance.