Companies can increase the overall effectiveness of their machines and help shape operations that are more flexible, reliable and energy-efficient using the new QuickStick® 150 Intelligent Conveyor System. As an extension of the Rockwell Automation independent cart technology portfolio, this technology presents an exciting opportunity to transform what is possible in facilities across the industrial landscape.
The QuickStick 150 Intelligent Conveyor System uses electro-magnetic force to deliver frictionless motion, enabling the movement of goods within machines or throughout a plant to occur with revolutionary speed and accuracy. With no moving parts such as gears, chains or belts used to generate motion, users can experience less downtime, reduced maintenance requirements and lower total cost of ownership.
Solutions can comprise of straight sections, turntables, shuttles, elevators, switches, curves and more - granting users the ability to craft dynamic paths that unlock the full potential of their operations.
By providing new levels of speed, precision and intelligence, the QuickStick 150 Intelligent Conveyor System helps provide a more efficient way for companies to move their products and achieve the flexibility to compete in the future marketplace.
QuickStick and Rockwell Automation are trademarks of Rockwell Automation Inc.
Published June 5, 2023