Change history tab
The
Change history
tab shows all changes committed to the repository for a local or shared project. Change history
lists the description of the changes, the date and time the changes were committed, and the email address of the user who checked in the changes. A unique ID identifies the set of changes in the repository. Open the Uncommitted changes
dialog box from the Change history
tab to view or discard uncommitted changes.To open
Change history
, open a local or shared project and then select File > Source control > Change history
. Provide Feedback