Immediate values

Immediate values

When you enter an immediate value (constant) in decimal format (for example, -2, 3) the controller stores the value by using 32 bits. If you enter a value in a radix other than decimal, such as binary or hexadecimal, and do not specify all 32 bits, the controller places a zero in the bits that you do not specify (zero-fill).
IMPORTANT: Zero-fill of immediate binary, octal or hexadecimal values less than 32 bits.
If you enter
The controller stores
-1
16#ffff ffff (-1)
16#ffff (-1)
16#0000 ffff (65535)
8#1234 (668)
16#0000 029c (668)
2#1010 (10)
16#0000 000a (10)
Integer Immediate Values
If you enter
The controller stores
Without any suffix
DINT
"U"
UDINT
"L"
LINT
"UL"
ULINT
Floating Point Immediate Values
If you enter
The controller stores
Without any suffix
REAL
"L"
LREAL
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal