Develop a confirmation dialog
Create a confirmation dialog that displays when you click a button. This project involves the creation of a custom method invocation.
NOTE:
Download a sample project:
ExampleApplication-DialogConfirmation.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
In
FactoryTalk Optix Studio
, select to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.Provide Feedback