Search
FactoryTalk Optix Studio Help Center
C# APIs reference
The description of the available C# APIs.
Development with C#
API to return known nodes
API to return nodes by searching
API to add or remove nodes
API to create objects
API to create variables
API to read or write field variables
API to keep field variables synchronized
API to write log messages
API to manage dynamic links
API to manage aliases
API to manage file and resource paths
Session activity log and audit
API to manage translations
Serial Port API
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.