Export a FactoryTalk Optix Application to a folder
Export a
FactoryTalk Optix Application
to a folder to use a shared folder to deploy the FactoryTalk Optix Application
to client machines that are not accessible by IP address. This is useful for clients that connect to the network intermittently, such as VPN clients or mobile clients.
TIP:
A folder can only contain one
FactoryTalk Optix Application
. Each FactoryTalk Optix Application
must use a separate folder. - InFactoryTalk Optix Studio, select the arrow next toSaveto open the pull-down menu and then selectExport FactoryTalk Optix Application to folder.
- InExport to folder,complete:
- Platform.Select the operating system of the client device.
- Location.Type the path to the location where you want to save theFactoryTalk Optix Application. Alternatively, select the folder icon to browse to the folder.
- SelectExport.
A progress windows displays while the
FactoryTalk Optix Application
is being exported. After the export has completed, a dialog appears to inform you that the FactoryTalk Optix Application
was successfully exported to the location specified.Provide Feedback