Events panel
Events are messages generated at runtime by an object to signal the occurrence of a situation of interest. Use the object editor to assign events to objects.
By default no events are assigned to objects.
Default event panel

Use the
Events
panel buttons to add events:Icon | Function |
---|---|
![]() | In the Events panel header: add an event of another object.Near an event: associate a method with the event. |
![]() | Delete the selected method. |
Provide Feedback