Main toolbar
The main toolbar at the top of of the user interface contains buttons that all views use.
Button | Function |
---|---|
![]() | Close a project. |
![]() | Create, open, or export a project. |
![]() | Cancel the last operation. |
![]() | Repeat the last operation. |
![]() | Open the project resource window for displaying, importing, or deleting project files (such as, images, videos, documents, certificates). |
![]() | Open the template library window and template variables. It contains both default and custom libraries. |
![]() | Open the .NET project to incorporate additional functionality using custom C# code. |
![]() | Open a configuration dashboard. Use the pull-down menu to select the configuration dashboard to open in the editor. |
![]() | Stop the application that is running on the client device. |
![]() | Compile, transfer, and run the application on the selected client device or emulator. Use the pull-down menu to select a different client device. |
Provide Feedback