Project view
A project contains the elements with which a
FactoryTalk Optix Application
is made. The
Project view
displays objects within a tree structure.Button | Function |
---|---|
Go back in the panel selection history. | |
Go forward in the panel selection history. | |
Divide the Project panel into two panels. | |
Create a node inside the selected node. | |
Remove the selected node and the nodes it contains. | |
Group the child nodes to hide them from the Project and make them non-editable. | |
Release child nodes of the group to display them in the Project and make them editable. | |
Open the object in the dedicated editor. This applies to only some object types. |
Provide Feedback