Enumerate items in Data controls objects

Enumerate items in Data controls objects

List items in Data control objects such as Data grids, by creating a dynamic link between the Model property and the target node.
TIP: For information about the available Data controls objects, see Data controls objects.
  1. In
    Project view
    , select a Data controls object.
    For example, select a Data grid object.
  2. In
    Properties
    , create a dynamic link between
    Model
    and a node that contains items that you want to enumerate.
    For more information about dynamic links, see Create dynamic links.
    For example, create a dynamic link between
    Model
    and a folder that contains objects that you want to enumerate.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.