Add a locale language to a localization dictionary

Add a locale language to a localization dictionary

Add locale languages to a localization dictionary so you can change the language displayed for an application at runtime.
  1. In
    Project view
    , expand
    Translations
    and double-click a localization dictionary.
  2. In the localization dictionary, in the
    Translation table
    view, select
    Add locale
    .
  3. Under
    Select the new locale
    , select a locale language and then select
    Checkmark
    .
  4. In
    New locales added
    , to add the locale to the displayed objects, select
    Yes
    .
A new column appears for the locale.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal