Program Composition Analysis Details

Program Composition Analysis Details

The
Program Composition
analysis dashboard displays the task schedules in the different programs of your project.
The program composition dashboard details the number of routines the task is present in and the type of program in which the task was developed:
  • Ladder Diagram (LD)
  • Function Block Diagram (FBD)
  • Structured Text (ST)
  • Sequential Function Chart (SFC)
It then identifies whether the task is inhibited, the name of the main routine and the fault routine and the class of the program. The parameters present in the task are also detailed, letting you know the usage of tags in the program. A count of each of the tags is provided:
  • Local tags
  • Input
  • Output
  • InOut
You can sort and filter the data in this dashboard. If you want to see the information in a different order, you can reorder the columns in the data table by dragging and dropping them as needed. To help you move around the analysis details page quickly, use keyboard shortcuts.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal