Access the AddOnInstructionDefinition Object
The
AddOnInstructionDefinition
object lets you customize instructions for sets of commonly-used logic, provides a common interface to this logic, and provides documentation for the instruction.Attribute | Data Type | Instruction within Standard Task | Instruction within Safety Task | Description |
---|---|---|---|---|
LastEditDate | LINT | GSV | None | Timestamp of the last edit to an Add-On Instruction. |
MajorRevision | DINT | GSV | None | Major revision number of the Add-On Instruction. |
MinorRevision | DINT | GSV | None | Minor revision number of the Add-On Instruction. |
Name | String | GSV | GSV | Name of the Add-On Instruction. |
RevisionExtendedText | String | GSV | None | Text describing the revision of the Add-On Instruction. |
SafetySignature ID | DINT | GSV | None | In a safety project, the ID number, date, and timestamp of an Add-On Instruction definition. |
SignatureID | DINT | GSV | None | 32-bit identification number of an Add-On Instruction definition. |
Vendor | String | GSV | None | Vendor that created the Add-On Instruction. |
Provide Feedback