Simultaneous Branch Diverge

Simultaneous Branch Diverge

The simultaneous diverge branch represents two or more alternate paths of execution.
In a simultaneous branch, all alternate paths are executed in parallel.
Available Languages
Ladder Diagram
Not Available
Function Block
Not Available
Sequential Function Chart
simultbranchdiverge1
Structured Text
Not Available
Description
A simultaneous branch represents steps or group of steps that occur at the same time (that is, an AND structure).
  • All branches execute.
  • All branch must finish before continuing with the SFC.
  • The controller checks the transition after the last step of each branch has executed at least once.
simultbranchdivergebig
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal