Error Codes

The Logix Designer application does not always display the full description.
Error Code (Hex)
Description
Display In Software
0001
Connection failure (extended error codes)
Same as description
0002
Insufficient resource
0003
Invalid value
0004
IOI syntax error (see extended error codes)
0005
Destination unknown, class unsupported, instance undefined or structure element undefined (see extended error codes)
0006
Insufficient packet space
0007
Connection lost
0008
Service unsupported
0009
Error in data segment or invalid attribute value
000A
Attribute list error
000B
State already exists
000C
Object model conflict
000D
Object already exists
000E
Attribute cannot be set
000F
Permission denied
0010
Device state conflict
0011
Reply will not fit
0012
Fragment primitive
0013
Insufficient command data
0014
Attribute not supported
0015
Too much data
001A
Bridge request too large
001B
Bridge response too large
001C
Attribute list shortage
001D
Invalid attribute list
Same as description
001E
Embedded service error
001F
Connection related failure (see extended error codes)
0022
Invalid reply received
0025
Key segment error
0026
Invalid IOI error
0027
Unexpected attribute in list
0028
DeviceNet error - invalid member ID
0029
DeviceNet error - member not settable
00D1
Module not in run state
Unknown error
00FB
Message port not supported
00FC
Message unsupported data type
00FD
Message uninitialized
00FE
Message timeout
00FF
General error (see extended error codes)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.