PLC and SLC Error Codes (.ERR)
Logix firmware revision 10.x and later provides new error codes for errors that are associated with PLC and SLC™ message types (PCCC messages).
This change lets RSLogix 5000 software display a more meaningful description for many of the errors. Previously the software did not give a description for any of the errors associated with the 00F0 error code.
The change also makes the error codes more consistent with errors returned by other controllers, such as PLC-5® controllers.
The table shows the change in the error codes from R9.x and earlier to R10.x and later. As a result of the change, the .ERR member returns a unique value for each PCCC error. The .EXERR is no longer required for these errors.
PLC and SLC Error Codes (hex)
R9.x And Earlier | R10.x And Later | Description | ||
---|---|---|---|---|
.ERR | .EXERR | .ERR | .EXERR | |
0010 | 1000 | Illegal command or format from local processor | ||
0020 | 2000 | Communication module not working | ||
0030 | 3000 | Remote node is missing, disconnected, or shut down | ||
0040 | 4000 | Processor connected but faulted (hardware) | ||
0050 | 5000 | Wrong station number | ||
0060 | 6000 | Requested function is not available | ||
0070 | 7000 | Processor is in Program mode | ||
0080 | 8000 | Compatibility file of processor does not exist | ||
0090 | 9000 | Remote node cannot buffer command | ||
00B0 | B000 | Processor is downloading so it is not accessible | ||
00F0 | 0001 | F001 | Processor incorrectly converted the address | |
00F0 | 0002 | F002 | Incomplete address | |
00F0 | 0003 | F003 | Incorrect address | |
00F0 | 0004 | F004 | Illegal address format - symbol not found | |
00F0 | 0005 | F005 | Illegal address format - symbol has 0 or greater than the maximum number of characters supported by the device | |
00F0 | 0006 | F006 | Address file does not exist in target processor | |
00F0 | 0007 | F007 | Destination file is too small for the number of words requested | |
00F0 | 0008 | F008 | Cannot complete request Situation changed during multipacket operation | |
00F0 | 0009 | F009 | Data or file is too large Memory unavailable | |
00F0 | 000A | F00A | Target processor cannot put requested information in packets | |
00F0 | 000B | F00B | Privilege error; access denied | |
00F0 | 000C | F00C | Requested function is not available | |
00F0 | 000D | F00D | Request is redundant | |
00F0 | 000E | F00E | Command cannot be executed | |
00F0 | 000F | F00F | Overflow; histogram overflow | |
00F0 | 0010 | F010 | No access | |
00F0 | 0011 | F011 | Data type requested does not match data available | |
00F0 | 0012 | F012 | Incorrect command parameters | |
00F0 | 0013 | F013 | Address reference exists to deleted area | |
00F0 | 0014 | F014 | Command execution failure for unknown reason PLC-3® histogram overflow | |
00F0 | 0015 | F015 | Data conversion error | |
00F0 | 0016 | F016 | The scanner is not available to communicate with a 1771 rack adapter | |
00F0 | 0017 | F017 | The adapter is no available to communicate with the module | |
00F0 | 0018 | F018 | The 1771 module response was not valid | |
00F0 | 0019 | F019 | Duplicate label | |
00F0 | 001A | F01A | File owner active - the file is being used | |
00F0 | 001B | F01B | Program owner active - someone is downloading or editing online | |
00F0 | 001C | F01C | Disk file is write protected or otherwise not accessible (offline only) | |
00F0 | 001D | F01D | Disk file is being used by another application Update not performed (offline only) |
Provide Feedback