Offset Results tab - FLEX I/O Analog

Offset Results tab - FLEX I/O Analog

This tab shows you the results of the offset calibration for FLEX I/O analog modules. You can see the results in the Status column.
offset
The steady-state deviation of a controlled variable from a fixed set point. In a linear function (y=mx+b), the parameter (b) is used to drive the dependent variable (y) to zero when the independent variable (x) is zero.
If the Status
column displays:
Then:
OK
Click Next to perform the gain calibration.
Error
Click Retry to repeat the process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal