Wiring Registration Sensors

The registration inputs to the servo module can support 24V or 5V registration sensors. These inputs should be wired to receive source current from the sensor. Current sinking sensor configurations are not allowed because the registration input common (IN_COM) is shared with the other 24V servo module inputs.
servo_wiringRegSensors
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.