Use tabbed tool windows

Use tabbed tool windows

When a tool window opens, it is added as a tab at the top of the main
Logix Designer
application window. Tabs can be undocked and moved as separate windows.
To use tabbed tool windows:
  1. To rearrange the order of the tabs, click and drag a tab to the left or right to place it before or after the other tabs.
  2. To undock a tab, drag and drop the tab away from the main
    Logix Designer
    application window.
  3. To close all tabs except the currently selected tab, right-click the tab and select
    Close All But This
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal