Select File Dialog Box

Use this dialog box to add project documentation translation to the project using a localization file.
Parameters
Parameter
Description
Look in:
Select the directory where the localization file resides.
Go to Last Folder Visited
Open the last visited folder. Enabled only if visited other folders and not at the default location for the dialog box.
Up One Level
Move up one level in the directory tree.
Create New Folder
Create a new folder in the current directory.
View Menu
Select folder view (thumbnails, tiles, icons, lists, or details)
File name:
Enter the name of the localization file to import.
Files of type:
Choose the file type to import.
Logix Designer
Unicode Import/Export Files (*.TXT) is the only available choice.
Import
Import the specified file.
Cancel
Cancel the import and close the Select File dialog box.
Help
View help about Select File dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.