Linear command

Choose this command to change the selected cam segments to linear type. When all cam segments are linear, this command is disabled.
NOTE:
Selecting a cam point also selects the cam segment which follows it, so that both the cam point and cam segment are highlighted.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.