Toolbars dialog box overview

From this dialog, you can select the toolbars that you want to be displayed in the main
Logix Designer
application window.
TIP:
If
FactoryTalk Security
is enabled, this dialog box may be disabled, depending on the levels of access that have been defined. For details about
FactoryTalk Security
see
FactoryTalk
Help:
Start > Programs >
Rockwell Software
>
FactoryTalk
Tools >
FactoryTalk
Help
.
This dialog includes these parameters:
Parameter
Description
Toolbars
A list of the available toolbars. Check the box of each toolbar you want to be displayed in the main
Logix Designer
application window.
Customize
The Language Element toolbar and Ladder Common Logic toolbar are customizable. Click this button to access the Customize Toolbar dialog box to customize these toolbars to your liking.
Close
Click this button to undo any changes you have made and close the Toolbars dialog box.
Note that clicking this button does not undo any changes you might have made in the Customize Toolbar dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.