Configure a Controller Fault Handler program
Configure a program as the Controller Fault Handler program. This program is executed when a controller major fault occurs, or a program fault is not handled by a fault routine.
IMPORTANT:
The program cannot be scheduled under a task.
To configure a Controller Fault Handler program
- From theEditmenu, chooseController Properties.
- Select theAdvancedtab.
- From theController Fault Handler Programmenu, choose the program to use.Note that a program must already exist in theController Organizer Controller Fault Handlerfolder in order for it to be available from this menu.
- SelectOK.
Provide Feedback