PlantPAx Tasking Model tasks and restrictions

Enabling
Use PlantPAx Tasking Model
creates tasks and puts task restrictions into effect.
Tasking Model tasks
Enabling tasking model moves scheduled programs to unscheduled programs, deletes existing tasks (programs and routines are not modified), and creates these four periodic tasks:
  • Fast
  • Normal
  • Slow
  • System
Tasking Model restrictions
Enabling tasking model prohibits these functions for tasks:
  • Creating
  • Deleting
  • Cutting
  • Pasting
  • Renaming
  • Editing task type
  • Editing task priorities
  • Editing Task Period property (For example, the Fast task cannot be edited to become faster than the Normal task.)
When
Use PlantPAx Tasking Model
is disabled, these restrictions are no longer in effect.
Changing controller types
When changing controller types, project content remains the same, except for existing rules that apply when changing controller types. When changing from a non
PlantPAx
controller to a
PlantPAx
controller, the Tasking Model option is disabled.
Import/Export
During imports and exports of
PlantPAx
projects, if the
Use PlantPAx Tasking Model
setting is enabled in the
PlantPAx
project, the same tasks and restrictions apply in the imported or exported project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.