Delete Custom Language Confirmation overview

Delete Custom Language Confirmation overview

To delete the custom language from the project, select:
  • Yes
    . To remove the custom language from the project.
  • No
    . To close the dialog box without removing custom language from the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.