Equipment Phase Properties - Configuration tab fields

Use the
Configuration
tab of the
Equipment Phase
Properties
dialog to create or modify the execution of the
Equipment Phase
. These options are available in the
Configuration
tab.
Name
Purpose
1
Prestate
Defines the prestate routine executed prior to the execution of any of the other state routines.
Prestate routines are optional routines to perform some failure detection, verify that all control modules are in the correct state, or execute other logic common to all state routines. When the equipment phase is in a state with no associated state routine (for example, IDLE, HELD, STOPPED), the Prestate routine continues to execute, but no state routine executes.
2
Fault
Defines the fault routine executed by the equipment phase whenever a major fault occurs within the equipment phase.
3
Inhibit equipment phase
Prevents the controller from executing this
Equipment Phase
. Clear the check box and the controller executes the
Equipment Phase
. The check box is clear by default.
4
Synchronize redundancy data after execution
Synchronizes data with the controller at the end of the phase execution. The check box is not shown for controllers that do not support redundancy. The check box is always enabled for controllers with redundancy enabled as long as the controller is not in Hard Run mode. The check box is disabled when redundancy is not enabled.
5
Initial state
The initial state can be:
  • ABORTED
  • COMPLETE
  • IDLE
  • STOPPED
Tip:
Equipment Phase
s must be configured to have an
Initial state
of IDLE to work with
Equipment Sequence
s.
6
Complete state immediately if not implemented or empty
Use this check box to signal the completion of a state any time the equipment phase transitions to a state where the state routine is not implemented.
7
Initial step index
Defines the initial value for the step index.
8
External sequencer loss of communication command
Defines the command to invoke if communication with an external sequencer that is currently an owner of the equipment phase fails.
  • <none>
  • ABORT
  • HOLD
  • STOP
9
External request hold action
Defines the action to take when an external request initiated using the
Equipment Phase
External Request (PXRQ) instruction is in progress and the equipment phase receives a HOLD command while in the RUNNING state. Choose from:
  • <none>
  • Clear. Aborts all external requests that are in progress.
10
Value assignment in an equipment sequence
Use the
Value assignment in an equipment sequence
check box to assign values for phase inputs and output in an
Equipment Sequence
based on the value of step input and outputs. When selected, all phase inputs use the value of the related step input.
11
Automatically assign the value of phase outputs to step outputs when the phase is:
Under
Automatically assign the value of phase outputs to step outputs when the phase is
, select a phase in which the
Equipment Sequence
uses the value of the related step output to evaluate the phase:
  • COMPLETE
  • STOPPED
  • ABORTED
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.