- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Add a simultaneous convergence
Use
to merge simultaneous execution paths back together.
Add Simultaneous Convergence

To add a simultaneous convergence
- On the Equipment Sequence Element toolbar, selectAdd Simultaneous Convergence
.
- Connect the convergence to a transition.
- Merge the paths of the simultaneous divergence by linking the final step of each path to the convergence.
Provide Feedback