SequenceManager and related components overview

Use the
SequenceManager
to model and execute sequential manufacturing processes using the
ControlLogix
features described in the following tasks:
  • Configure the coordination of Equipment Phase execution using the
    Equipment Sequence
    Editor.
  • Execute Equipment Sequence programs using
    ControlLogix
    .
  • Monitor and manage running Equipment Sequences using the
    Logix Designer
    application.
  • Enable operators to monitor and manage running Equipment Sequences and Equipment Phases by adding
    SequenceManager
    ActiveX controls to
    FactoryTalk View SE
    displays.
  • Subscribe and collect generated sequence events using
    SequenceManager
    Event Client Service and
    SequenceManager
    Event Archiving Service.
The following diagram illustrates the components that are part of the
SequenceManager
and their responsibilities.
L5K_SeqMgr_Comp
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.