- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Move Equipment Sequence elements
Cut, paste, and move
Equipment Sequence
elements for use in another location in the current diagram.To move
Equipment Sequence
elements:To cut an
Equipment Sequence
element:- Select one or more elements to cut.
- On the Menu bar, sekectEdit > Cut Element.
- Paste the cut element(s) into the desired location.TIP:CutEquipment Sequenceelements by using these methods:
- Right-click a step and selectCut Element.
- Select a step and use the keyboard shortcutCtrl + X.
- Select a step and use theCutbutton on the main toolbar.
To paste an
Equipment Sequence
element:- Select one or more elements.
- On the Menu bar, selectEdit > Paste.
- Paste the cut or copied element(s) to the desired location.TIP:Also paste anEquipment Sequenceelement using one of these methods:
- Right-click a step and selectPaste.
- When the sequence editor has focus, use the keyboard shortcutCtrl + V.
- Select a step and use thePastebutton on the main toolbar.
To move elements in an
Equipment Sequence
diagram:- Select one or more elements to move.
- Drag the element to the desired location.
- Stop dragging the element to complete the move.
Provide Feedback