Create a simultaneous branch
A simultaneous branch is a type of branch with two or more parallel paths where all paths within the branch are selected to execute at the same time. This is also known as a non-conditional (AND) branch.
Simultaneous branch requirements
Following is a summary of requirements for creating paths and connecting elements in a simultaneous branch.
- Each execution path in a simultaneous branch must start with a step.
- Each execution path in a simultaneous branch must end with a step before connecting a simultaneous convergence and mergeing the paths.
- A simultaneous convergence must be followed by a transition.
To create a simultaneous branch:
To create a simultaneous divergence:
- On the Equipment Sequence Element toolbar, selectAdd Simultaneous Divergence
.
- Link the divergence to a preceding transition.
- Add execution paths to the divergence:
- Add and connect a step or a step and transition pair to the divergence to create a separate execution path.
- Repeat to create additional execution paths as needed.
- Add and connect additional steps and transitions to each execution path as needed.
- Verify each execution path ends with a step.
- On the Equipment Sequence Element toolbar, selectAdd Simultaneous Convergence
.
- Connect the convergence to a transition.
- Merge the paths of the simultaneous divergence by linking the final step of each path to the convergence.
Provide Feedback