Equipment Sequence Properties - Configuration tab fields
Use the
Configuration
tab of the Equipment Sequence Properties
dialog box to create or modify the execution of the Equipment Sequence. The following options are available in the Configuration
tab.
Name | Purpose | |
![]() | Inhibit equipment sequence | Select the Inhibit equipment sequence check box to prevent the
controller from executing this Equipment Sequence . Clear the check box and the
controller will execute the Equipment Sequence . The check box is clear by
default. If the Equipment Sequence is inhibited, n Equipment Sequence icon
displays in the Controller Organizer with the inhibited
decorator: ![]() |
![]() | Retain sequence ID when resetting sequence | Select this option to retain the sequence ID when resetting the Equipment Sequence . If this is not selected, a RESET command clears the Sequence ID value of an Equipment Sequence . |
![]() | Generate sequence events | Select this option to generate sequencing events that record the manufacturing process. This includes operator commands, changes in sequence attributes, and changes in sequencing parameters and step tag values. |
![]() | Unit ID | The Unit ID is an integer value assigned to represent the equipment unit the sequence is coordinating. This value is recorded with sequence events to identify the equipment coordinated. |
For parameters and step tags using initial value as the value source: | ||
![]() | When starting sequence |
|
![]() | When resetting sequence |
|
OK | Select to accept edits. If all attributes are valid, the modified attributes save for the current Equipment Sequence and the dialog box closes. OK and Apply are not available if the dialog box contains invalid data. | |
Cancel | Select to cancel edits and close the Equipment Sequence Properties dialog box. | |
Apply | Select to apply edits and continue editing in the Equipment Sequence Properties dialog box. Applying edits runs the same validation as clicking OK . |
Provide Feedback