Routine Properties dialog box

The
Routine Properties
dialog box sets routine properties for the
Equipment Sequence
.
TIP: To open the
Routine Properties
dialog box, right-click the
Sequence Editor
pane and select
Properties
.
Use the
General
tab to:
  • Review routine information such as the name, type, which
    Equipment Sequence
    , and the number of steps in the
    Equipment Sequence
    .
  • Enter an optional description of the routine for the
    Equipment Sequence
    .
Use the
Sheet Layout
tab to:
  • Specify or change the sheet size for the selected
    Equipment Sequence
    .
  • Specify or change the page layout options (landscape or portrait) for the
    Equipment Sequence
    .
    TIP:
    • Tip: The
      Sheet Layout
      tab only displays on the Routine Properties dialog box for unprotected sequence routines.
    • The
      Source Not Available
      appears when a user attempts to access a protected routine without the source protection key.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.