- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Function Block Routines
Each language has different routine properties. Function Block Routines have general properties which identify the name of the routine, the program to which the routine belongs, and the number of sheets contained in the routine and sheet layout properties that define the sheet size and orientation.
You edit routine properties using the
Routine Properties
dialog box. To access the Routine Properties
dialog box, right click the routine whose properties you want to change from the Controller Organizer
or Logical Organizer
, and choose Properties
.Provide Feedback