Use drag-and-drop to schedule and unschedule programs in the Controller Organizer

Use drag-and-drop to schedule and unschedule programs in the Controller Organizer

You can use drag-and-drop in the
Logical Organizer
to create a logical model that is organized in terms of procedures, objects, functions, equipment, or other more natural terms and concepts. You can then use drag-and-drop to apply this logical model in the
Controller Organizer
.
TIP:
If FactoryTalk Security is enabled, you need FactoryTalk Security permissions to create and delete items in the
Controller Organizer
and the
Logical Organizer
.
Apply the logical model to the Controller Organizer
You can schedule and unschedule programs and routines in the
Controller Organizer
by creating your logical model in the
Logical Organizer
, and then dragging part or all of your logical model from the
Logical Organizer
to the
Controller Organizer
. For example, you can create a
Logical Organization
of programs for Mixers as shown below. In the
Controller Organizer
, the programs are initially unscheduled.
NOTE:
Reorganize_LO_to_CO_1_v31
You can then drag-and-drop Mixers from the
Logical Organizer
to the
Controller Organizer
to schedule the programs under MainTask. Note that Mixers is a folder in the
Logical Organizer
, and does not appear in the
Controller Organizer
.
NOTE:
Reorganize_LO_to_CO_4_v31
Description
Cursor
Move cursor that appears where you can drop the item (click and drag)
Copy cursor that appears where you can drop a copy of the item (
Ctrl+click
and drag)
NOT cursor that appears where you cannot drop an item.
Restrictions:
  • You cannot move a Safety program when in Safety Lock. If you select multiple programs, and any of them is a Safety program, only the standard programs are moved in Safety Lock. The system log a warning that the Safety programs are not moved.
  • Drag-and-drop is not allowed if the system is in Hard Run or has a major fault.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal