Use the right mouse button

Click the right mouse button on an item for quick access to menu options. Different options are available depending on which items is right-clicked. For example, with a program file icon selected, click the right mouse button to bring up a menu with options that relate to the program file.
When a menu is visible, use the left mouse button to click any item. This immediately carries out the function or displays a functional dialog box. Enter the required parameters in the dialog box to complete the specific task.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.