Routine Properties dialog box - Sheet Layout tab overview (Sequential Function Chart routine)
From this dialog, specify the sheet size and orientation for the selected sequential function chart routine.
TIP:
You cannot modify the sheet layout while online, but you can view the current layout.
Parameter | Description |
---|---|
Sheet size | Enter the sheet size to use for this sequential function chart routine. |
Orientation | Click the sheet orientation to use for this sequential function chart routine. Choose from Landscape or Portrait. Upon installation of the Logix Designer application, the orientation defaults to Portrait. However, choosing a different orientation, the next time a routine is created, that orientation becomes the default for the new routine. |
OK | Click to apply edits and close the Routine Properties dialog box. |
Cancel | Click to cancel edits and close the Routine Properties dialog box. |
Apply | Click to apply edits and continue editing in the Routine Properties dialog box. |
Help | Click for help on the Sheet Layout tab. |
Provide Feedback