- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Referenced component requires additional properties
This validation error appears in the
Errors
box of the Output
window:Error: <LockedComponentName>: Locked component requires <ReferencedComponentType> <ReferencedComponentName> to have <Required Properties>
The error indicates that a locked routine or Add-On Instruction references a component that was modified since the routine or Add-On Instruction was locked, and the locked component and the referenced component may no longer be compatible.
To correct this error, edit the referenced component to match the properties identified in the error message. Unlocking and re-locking the locked component corrects this error, particularly when the error occurs when converting a project to a newer version of the
Logix Designer
application.Provide Feedback