Select a file and function
The external routine can call a file or function.
To select a file and function:
- In the Controller Organizer, right click the active routine and chooseProperties.
- InExternal Routine DLL, enter the name of the .dll file the external routine calls.
- Click theBrowsebutton to search for a specific file.
- InFunction, enter the function within the .dll file the external routine calls.
- Click
to choose a specific function.
- ClickOKto close the Routine Properties dialog.
Provide Feedback