Overview
This course provides you with the skills necessary to maintain and troubleshoot FactoryTalk® View Machine Edition (ME) applications that run on PanelView™ Plus 7 terminals. This course provides opportunities to work with both the hardware and software.
During class, you will gain the following hands-on skills:
• Prepare a PanelView Plus 7 terminal for operations
• Create tags and test data in a FactoryTalk View ME application
• Modify graphic displays in an application
• Transfer runtime files to and from a terminal
• Diagnose issues and troubleshoot a terminal