Across the manufacturing value chain, a new framework for improving performance is emerging -- one that connects digitally enabled factory processes to closed-loop continuous traditional process improvement (CPI).
Digital performance management (DPM) is an industrial information solution built in PTC’s ThingWorx that leverages familiar lean principles to transform how factories achieve higher levels of operational excellence. While the principles and many of the component tools are well established, the way they are brought together is groundbreaking. DPM collects data from automation, and operator engagement identifies production bottlenecks and delivers operational equipment efficiency (OEE) calculations. Combined with time loss pareto analyses, DPM enables better decisions on where to invest scarce resources in a closed-loop continuous process improvement (CPI) initiative. DPM helps identify hidden opportunities to enhance performance that can lead to double digit improvements.
Plenty of Data, Not Enough Insight
The problem with data is no longer a lack of availability, poor accuracy, or timeliness. Factory executives are awash in timely, accurate data. Rather, there’s a significant gap between data and useful insight. Many manufacturing organizations have a hard time figuring out how to manage, sort, organize, curate and deliver valuable insight. They need their data to enable and support better decision-making.
DPM ingests operating data and then analyzes and presents it in ways to make problem identification easier, and selection among corrective action alternatives more efficient.
Closed Loop Problem Solving and Production Operations
Identifying bottlenecks in a consistent, repeatable way is difficult to do manually and is labor-intensive. DPM for PTC provides a set of tools that largely automates the collection of data and identification of the production line’s pacesetting operation.
To understand DPM, think of these steps:
- Monitor: Constantly measure what’s going on in a factory line.
- Focus: Find the production pacesetter. Identify and rank bottlenecks.
- Prioritize: Identify the highest impact performance issues that demand focus.
- Analyze: Determine root causes and characterize the sources of loss in the operation.
- Improve: Put a plan in place to fix it.
- Confirm: Monitor the fix and make sure the plan fixes the problem.
- Repeat