Deploy a FactoryTalk Optix Application from a folder
To deploy a
FactoryTalk Optix Application
from a folder on a network share or a USB drive, move the file to the client device and run the file.If the client device is… | Then… |
---|---|
Windows | Double-click the file FTOptixRuntime.exe . |
Linux | Insert the USB key in a USB port on the client device. |
Debian | Run the FTOptixRuntime file using the shell command. |
Provide Feedback