Deploy a FactoryTalk Optix Application over the network
To deploy a
FactoryTalk Optix Application
to a client device you must configure the FactoryTalk Optix Application
for the client operating system and then run the application on the client device Rockwell Automation
client devices automatically run a FactoryTalk Optix Application
upon deployment. Other client devices require that you manually start the application on the device or configure the application for automatic startup.If a
FactoryTalk Optix Application
is already running on a client device, deploying another FactoryTalk Optix Application
stops the other application.If
FactoryTalk Optix Studio
cannot connect to the IP address of the client device on the network, the FactoryTalk Optix Application
can be deployed by exporting the FactoryTalk Optix Application
to a folder or USB drive.Prerequisites
Before deploying the
FactoryTalk Optix Application
to a client device, ensure that the client device has the FactoryTalk Optix Application Update Service
started and that the client device has a valid license.
NOTE:
If the client device is not licensed, the
FactoryTalk Optix Application
runs in demo mode, which stops running automatically after two hours.To deploy a FactoryTalk Optix Application
FactoryTalk Optix Application
- Set the active client
- SelectRunto display the pull-down menu.
- Select the client device configuration from the list.
- Run the application.
- SelectRun.
- Enter the password for the user account identified in the client device configuration and then selectOK.
- (optional) To stop the application an a client device, set the client device that runs the application as active and then selectStop.
Provide Feedback