Output panel
The
Output
panel contains buttons to perform tasks on the panel. Button | Function |
---|---|
Select to display or hide the error messages of maximum severity. | |
Select to display or hide the error messages of minimum severity. | |
Select to display or hide information messages. | |
Select to display or hide verbose 1 messages. | |
Select to display or hide verbose 2 messages. | |
Open the output logs folder. For more information, see System log | |
Delete all messages, regardless of display selected, from the output panel.
TIP:
Messages are not deleted from the log files.
|
Column Name | Description |
---|---|
- | Message severity level = error of maximum severity = error of minimum severity = information notices |
Code | (Only for FactoryTalk Optix predefined messages) Message ID code. |
Timestamp | The time the system logged the message. |
Category | Category of the FactoryTalk Optix Platform message or module that generated the message. |
Object | The element referenced by the message, if applicable. |
Message | Message content. |
TIP:
Select the arrow in a column heading to sort messages in ascending or descending order according to the data in that column.
In the
Category
column, select to filter the displayed messages by category.Provide Feedback