- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Quick start: develop a sample project
Develop, compile, and run a sample HMI
FactoryTalk Optix Application
that demonstrates different capabilities of FactoryTalk Optix Studio
.
TIP:
- At any point of this tutorial, you can test your application by selectingRun
- Throughout this tutorial, save changes periodically by pressingor selecting from the toolbar.You can use Git to version-control your project. For more information, see Version control.
- You can download, unzip, and open the finished project to investigate its components and settings: QuickStart.zip
Prerequisites
- To develop the project
- Configure and brand the main window:
- Configure panels and tab-based navigation:
- Configure dynamic graphic objects:
- Configure variables and add temperature controls:
Provide Feedback